GetMaterialList

Returns a list of Materials in a multi-dimensioned array.
Syntax
vResult
=
MaterialSvr
.
GetMaterialList
(
MaterialFilter
As
MaterialFilterEnum
,
FilterValue
As String)
The
GetMaterialList
method syntax has these parts:
Part
Description
vResult
The data returned by the Material Server.
MaterialSvr
Instance of the MaterialServer to which the method is directed.
MaterialFilter
An enumeration representing a set of pre-defined filters:
0 = GetAllMaterials
1 = GroupName
2 = ClassificationName
3 = MaterialName
FilterValue
A string representing the filter value.
Where
vResult
is:
Part
Description
vResult
Is a two-dimensional array containing
<
EmptyArray
> | <
MaterialData
>
MaterialData
Array Element [0] = Pkid
Array Element [1] = Name
Array Element [2] = Description
Array Element [3] = ControllerID
Remarks
In order to test for an empty array, you must test the upper and lower bounds of the
vResult
array. If both bounds are zero, then the array is empty and can be treated as such.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal