GetContainerStateList

Returns a list of ContainerStates in a multi-dimensioned array.
Syntax
vResult
=
MaterialSvr
.
GetContainerStateList
()
The
GetContainerStateList
method syntax has these parts:
Part
Description
vResult
The data returned by the Material Server.
MaterialSvr
Instance of the MaterialServer Batch Interface to which the method is directed.
Where
vResult
is:
Part
Description
vResult
Is a two-dimensional array containing
<
Empty Array
> | <
ContainerStateData
>
ContainerStateData
Array Element [0] = PKid
Array Element [1] = Name
Array Element [2] = Description
Array Element [3] = ControllerID
Remarks
In order to test for an empty array, you must test the upper and lower bounds of the
vResult
array. If both bounds are zero, then the array is empty and can be treated as such.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal