GetContainerState

Returns a ContainerState object with its properties populated with corresponding data from the material database, based on the ContainerState Name.
Syntax
Set
object
=
MaterialSvr
.
GetContainerState
(ByVal
sName
As String,
UseCollection
As Boolean)
The
GetContainerState
method syntax has these parts:
Part
Description
object
Reference to a valid ContainerState object.
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
sName
Represents the name of the ContainerState.
UseCollection
True:
Attempts to locate the specified ContainerState in a pre-populated collection. If no collection is present, one is created and the record is read from the collection.
False:
Reads the record directly from the database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal