GetContainersHavingMaterial

Returns a collection of 1 to N MaterialContainer objects.
Syntax
Set
object
=
MaterialSvr
.
GetContainersHavingMaterial
(
IMaterialID
As Long)
The
GetContainersHavingMaterial
method syntax has these parts:
Part
Description
object
Reference to a valid MaterialContainers collection object.
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
MaterialID
Represents the ID of the Material.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal