GetContainerList
Returns a list of Containers in a multi-dimensioned array.
Syntax
vResult
= MaterialSvr
.GetContainerList
(ByVal ContainerFilter
As ContainerFilterEnum , ByVal FilterValue
As String)The syntax has these parts:
GetContainerList
methodPart | Description |
---|---|
vResult | The data returned by the Material Server. |
MaterialSvr | Instance of the MaterialServer Batch Interface to which the method is directed. |
ContainerFilter | An enumeration representing a set of pre-defined filters. Enumeration: 0 = GetAllContainers 1 = GetContainersNotInStorageLocation 2 = GetContainersInStorageLocation 3 = GetIndependantContainersAndStorageLocations 4 = GetAllContainersInAllStorageLocations |
FilterValue | A string representing the Storage Location name, used by the ContainerFilter to filter on. |
Where
vResult
is:Part | Description |
---|---|
vResult | Is a two-dimensional array containing < Empty Array > | <ContainerData > |
ContainerData | Array Element [0] = ControllerID Array Element [1] = ConatinerName |
Provide Feedback