GetContainerByControllerID

Returns a Container object populated with the specified Container data from the material database, based on the ControllerID.
Syntax
object
=
MaterialSvr
.
GetContainerByControllerID
(ByVal
ControllerID
As Long)
The
GetContainerByControllerID
method syntax has these parts:
Part
Description
object
Reference to a valid Container object.
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
ControllerID
ControllerID of the Container being requested. It is expected that the program using this interface know the ControllerID for the data entity it wants to access.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal