DistributeSubLot

Distributes all or a portion of a Lot’s total quantity to a Container. It can also be used to distribute or redistribute portions of existing SubLots to other Containers.
Syntax
SubLot
.
DistributeSubLot
(ByVal
Quantity
As Double, ByVal
Container
As Long, [ByVal
Label
As String, [
ActivityDescription
As String])
The
DistributeSubLot
method syntax has these parts:
Part
Description
SubLot
Instance of the SubLot object to which the method is directed.
Quantity
Represents the Quantity of the SubLot to distribute.
Container
Represents the ContainerID of the Container that is being distributed to.
Label
Represents the Label that can be applied to the distributed SubLot. (
Optional
)
ActivityDescription
Adds descriptive text to the activity journal for this operation. (
Optional
)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal