DeleteSubLot
Deletes a SubLot record from the material database.
Syntax
MaterialSvr
.DeleteSubLot
(SubLot
As SubLot, [ActivityDescription
As String])Lot
.DeleteSubLot
(SubLot
As SubLot, [ActivityDescription
As String])The method syntax has these parts:
DeleteSubLot
Part | Description |
---|---|
MaterialSvr | Instance of the MaterialServer Interface to which the method is directed. |
Lot | Instance of a Lot object to which the SubLots are to be deleted from. |
SubLot | An instance of a SubLot object. |
ActivityDescription | Adds descriptive text to the activity journal for this operation. ( Optional ) |
Remarks
SubLots that are deleted do not have the effect of returning any of the remaining SubLot quantity back to the Lot in which the SubLot was created. In effect, the SubLot and any quantity are deleted from inventory.
This method is available in two locations within the material object model: the MaterialServer object and the Lot Object. Use the one that is appropriate for your needs.
Provide Feedback