DeleteMaterialClass

Deletes a MaterialClass record from the material database.
Syntax
MaterialSvr
.
DeleteMaterialClass
(
MaterialClass
As MaterialClass)
The
DeleteMaterialClass
method syntax has these parts:
Part
Description
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
MaterialClass
An instance of a MaterialClass object.
Remarks
A MaterialClass can only be deleted if there are no Materials using it. There is no provision in this method to override this functionality or disassociate the Materials that are using the MaterialClass.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal