DeleteMaterial

Deletes a Material record from the material database.
Syntax
MaterialSvr
.
DeleteMaterial
(
Material
As Material, [
ActivityDescription
As String])
The
DeleteMaterial
method syntax has these parts:
Part
Description
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
Material
An instance of a Material object.
ActivityDescription
Adds descriptive text to the activity journal for this operation. (
Optional
)
Remarks
Along with the deletion of the Material, all associated MaterialProperties, LotProperties, Lots, and SubLots are deleted from the database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal