DeleteLotState

Deletes a LotState from the material database.
Syntax
MaterialSvr
.
DeleteLotState
(
LotState
As LotState)
The
DeleteLotState
method syntax has these parts:
Part
Description
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
LotState
An instance of a LotState object.
Remarks
A LotState can only be deleted if no Lots are using it. There is no provision in this method to override this functionality, nor is there a way to unassociate the Lots that are using the LotState.
The ‘Ready To Use’ LotState is system-defined and cannot be deleted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal