DeleteContainerMaterial

Deletes a ContainerMaterial from the material database.
Syntax
Container
.
DeleteContainerMaterial
(
ContainerMaterial
As ContainerMaterial, [
ActivityDescription
As String])
The
DeleteContainerMaterial
method syntax has these parts:
Part
Description
Container
Instance of the Container object to which the method is directed.
ContainerMaterial
An instance of a ContainerMaterial object.
ActivityDescription
Adds descriptive text to the activity journal for this operation. (
Optional
)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal