DeleteContainer
Deletes a Container from the material database.
Syntax
MaterialSvr
.DeleteContainer
(Container
As Container, [ActivityDescription
As String])The
DeleteContainer
method syntax has these parts:Part | Description |
---|---|
MaterialSvr | Instance of the MaterialServer Interface to which the method is directed. |
Container | An instance of a Container object. |
ActivityDescription | Adds descriptive text to the activity journal for this operation. ( Optional ) |
Remarks
Along with the deletion of the Container, all associated ContainerProperties, ContainerPriorities, ContainerMaterials and Promises are deleted from the database when this method is executed.
Containers cannot be deleted if they are in use by any SubLot in the material database.
The ‘Virtual Container’ is a system-defined Container that cannot be deleted via this method or any other means.
Provide Feedback