Material Server API overview
The Material Server API is the interface between the Material Server, the Material Editor, and
FactoryTalk Batch
. Using the material object model (MOM) you can develop a custom user interface application.The material object model provides the interface to the Material Server:

Provide Feedback