Verifying the recipe

Once you have added all the material-enabled phases to the recipe, verify the recipe before the recipe is ready to run.
  1. From the
    File
    menu, select
    Verify All Recipes
    .
    If you are prompted to save, click
    Yes
    .
  2. When the verification is complete, click
    Accept
    , and then click
    Close
    . If prompted, enter auditing comments, if desired, and click
    OK
    .
  3. Exit the
    FactoryTalk Batch
    Recipe Editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal