Linking phase groups
Use phase link groups to identify phases that communicate and work together, such as the XFR_OUT and XFR_IN phases that transfer the sweetcream mixture from the mixer to the freezer. In the Equipment Editor, both the XFR_OUT and XFR_IN phases are configured with one message partner, which indicates that these phases must communicate with one other phase to work properly.

Equipment Editor: Phase Message Partners
In the Recipe Editor, you must create a phase link group at the procedure level to complete the association.
- SelectXFR_IN:1in either the Procedure Hierarchy or the SFC view.
- From theLinkmenu, selectLink Groups. ThePhase Link Groupdialog box opens.
- Click the Group 1 column heading to select the Group 1 column, and then click theAddbutton.
- ClickOK.
- ClickXFR_OUT:1.
- From theLinkmenu, selectLink Groups. ThePhase Link Groupdialog box opens.
- Select the Group 1 column, click theAddbutton, and then clickOK.
Provide Feedback