Enabling dynamic unit allocation

To support the flexibility of the two units within NORTH_PARLOR process cell, you want to enable dynamic unit allocation, which will provide more binding options.
  1. From the
    View
    menu, select
    Options
    . The
    Options
    dialog box opens.
  2. If necessary, enable
    Support Dynamic Unit Allocation
    , and then click
    Apply
    .
  3. Save the unit procedure. If prompted, enter auditing comments, if desired, and click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal