Creating recipe formula parameters
Because you want to defer the amounts of the materials at this level in the recipe, you need to add formula parameters. You will enter default amounts at the procedure level and the operator will have an opportunity to change the amount when the batch is added to the batch list.
- From theRecipemenu, selectRecipe Parameters/Reports. TheProcedure Propertiesdialog box opens.
- Click theAdd Parameterbutton.
- In theNamebox, typeCOCOA_AMT.
- In theMaxbox, type500.
- In theEnum/EUbox, typeKG.
- SelectScalable.
- Click theNewbutton, and then addHAZELNUT_AMTwith the same values.
- ClickOK.
Provide Feedback