Create a material-based operation

  1. Select
    Start > Rockwell Software > Recipe Editor
    . If the
    Recipes Requiring Verification
    dialog box opens, click
    Cancel
    .
  2. IMPORTANT:
    Administrator privileges are required to perform this procedure.
    Select
    File
    >
    New Top Level
    . The
    New
    dialog box opens.
    FTBMM_GRG_new
  3. Select
    Operation
    , and then click
    OK
    . The
    Unit Requirement
    dialog box opens.
    FTBMM_GRG_equipment_requirements
    You want the recipe to run on both units in the process cell.
  4. Select
    Class-Based
    , select
    MBR_FREEZER_CLS
    , and then click
    OK
    . The initial and final steps of the new operation display in the SFC View.
    FTBMM_GRG_recipe_sfc_3
  5. Select the initial step, and then click the
    Add Step
    button, select
    MBR_ADD
    , and then click
    OK
    .
  6. Click the
    Add Parallel
    button, select
    RECIRC
    , and then click
    OK
    .
  7. Select the last transition, click the
    Add Step
    button, select
    TEMP_CTL
    , and then click
    OK
    .
  8. Click the
    Add Parallel
    button, select
    RECIRC
    , and then click
    OK
    .
  9. Select the last transition, click the
    Add Step
    button, select
    MBR_ADD
    , and then click
    OK
    .
  10. Click the
    Add Parallel
    button, select
    RECIRC
    , and then click
    OK
    .
  11. Select the last transition, click the
    Add Step
    button, select
    MBR_DUMP
    , and then click
    OK
    .
  12. Select
    Recipe
    >
    Header Data
    , and then enter the following:
    • Procedure Identifier:
      MCLS_CHOCOLATE_HAZELNUT_OP
    • Author:
      Your Name
    • Product Name:
      CHP-100
    • Batch Size Default:
      5000
    • Batch Size Max:
      10000
    • Units of Measure:
      KG
    • Estimated Duration:
      55
    • Procedure Description:
      Chocolate Hazelnut Premium Ice Cream
  13. Click
    OK
    , and then click
    Proceed
    . If prompted, enter auditing comments, if desired, and then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal