Questions to ask about the material database

Some of the questions you will want to answer before you move forward in the planning phase are:
  1. Does the current material data include the following characteristics?
    • States
    • Types
    • Classes
    • Materials
    • Properties
    • Lots/Sublots
    • Locations
    • Independent containers
  2. How will the data fields be mapped from the existing data to the material database?
  3. In what form is the material data?
    • Doesn’t exist
    • Paper
    • Electronic
  4. Will the data be entered manually or programmatically?
  5. What method of synchronization will be used?
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal