Determining the system requirements
The system requirements for a Material Manager implementation are determined by the FactoryTalk Batch system configuration. A FactoryTalk Batch system is a group of networked computers on which one or more FactoryTalk Batch components run. Material Manager can be implemented in a number of different configurations: with FactoryTalk Batch, with
eProcedure
, and with various combinations of each of these. Each of these configurations represents a FactoryTalk Batch system. The system requirements will include the number and type of computers you need, operating systems required on each computer, and the security scheme to be implemented.
Provide Feedback