Changing list view properties
The List View Properties area contains the following options to change the appearance and behavior of items seen in a list view.
- "Hot" list selection– If selected, an item is automatically highlighted and selected when the cursor remains over the item for a certain period of time.
- List information tips– If selected, single-line tips appear when you move the cursor over a button or field. See Editing information tips for more information.)
- Flat scroll bars– If selected, scroll bars appear 2‑dimensional. If disabled, scroll bars have a 3‑dimensional appearance (Windows default). The following figure illustrates both the default (on the left) and flat (on the right) scroll bars:
- Header drag and drop– If selected, users can click and drag a header from one location to another in order to rearrange the columns.
- Header "hot" tracking– If selected, an item is automatically highlighted but not selected when the cursor moves over a header item. You must still click the item at least once to activate it.
- Subitem images
Provide Feedback