Changing fonts

The Material Editor defaults to the current Windows fonts. You can change the display font.
  1. On the
    General
    tab in the
    User Preferences
    dialog box, select
    Use application font
    .
  2. Select the
    Font
    tab.
    FTBMM_ED_user_preferences_fonts
  3. Click the
    Select Font
    button. The
    Font
    dialog box opens.
  4. Select the desired font, style, and size from the appropriate lists, and then click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal