Creating storage locations

Storage locations represent the locations of actual material storage containers. When adding new locations, you must add a record of the location before you can configure it.
  1. In the Hierarchy pane, right-click
    Locations
    , and then select
    New Material Storage Location
    . The
    Create Material Storage Location
    dialog box opens.
    FTBMM_ED_Storage Location_New
  2. In the
    Name
    box, type a unique name for the material.
  3. In the
    Description
    box, type a detailed description of the material.
  4. In the
    Controller ID
    box, type a unique number if desired. If left at 0 (zero), the
    Controller ID
    defaults to the next numeric value in sequence.
  5. Click
    OK
    to save the new location and close the dialog box.
  6. In either the Hierarchy or Detail pane, right-click the storage location, and then select
    New Material Storage Container
    .
  7. Configure the material storage containers for this storage location. (See Configuring storage containers for more information.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal