Removing a material

Removing a material merely unassigns the material from that container. The material definition still exists in the material database.
  1. There are three methods you can use to move materials from the
    Configured Materials
    list to the
    Source Materials
    list.
    • To remove a single material, select the material in the
      Configured Containers
      list, and then click the
      Remove
      button.
    • To remove more than one material, select a material in the
      Configured Materials
      list, hold down either the shift key or the ctrl key, select other materials to remove, and then click the
      Remove
      button.
    • To remove all the materials in the
      Configured Materials
      list, click the
      Remove All
      button.
  2. Click
    Apply
    to save the changes, or click
    OK
    to save the record and close the dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal