Distributing a lot
When you distribute a sublot of material, the distributed sublot appears with the
Label
, Container
, and Amount
distributed in the inventory of the selected storage container and also in the materials inventory.- From theEdit Material Storage Containerdialog box, select the record row to distribute, and then click theDistributebutton. TheDistribute Lotdialog box opens.
- In theLabelbox, type a unique label name for the sublot.
- In theQuantitybox, type the amount to distribute.
- From theStorage Containerlist, select a container to use for storing the distributed amount.
- ClickOKto return to theInventorytab. If you distributed the lot into the container in which you are working, the new sublot displays, with theLabel,Container, andAmountdistributed in the inventory.
Provide Feedback