Editing container properties
- From theEdit Material Storage Containerdialog box, select a record number to edit and click theEdit Propertybutton.
- Modify the container property as needed, and then clickOK.IMPORTANT:If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
- ClickApplyto save the changes, or clickOKto save the record and close the dialog box.
Provide Feedback