Configuring container materials
From the
Materials
tab you can add or remove source materials, by group or individually, to the container.- From theEdit Material Storage Containerdialog box, select theMaterialstab.
- There are three methods you can use to move materials from theSource Materialslist to theConfigured Materialslist.
- To add a group of materials, select a group from theSource Materialslist, and then click theAdd Classbutton. All the materials assigned to that class are added to theConfigured Materialslist.
- To add a single material, expand a material group to display the materials. Select a material, and then click theAddbutton.
- To add all the source materials to the configured materials, click theAdd Allbutton.
- ClickApplyto save the changes, or clickOKto save the record and close the dialog box.
Provide Feedback