Changing inventory quantity

  1. From the
    Edit Material Storage Container
    dialog box, select the
    Inventory
    tab. The list of sublots for the storage container displays.
    FTBMM_ED_Storage Container_Inventory tab
  2. Select the record row to edit, and then click the
    Edit Distribution
    button. The
    View Lot Distribution
    dialog box opens.
    FTBMM_ED_Storage Container_View Lot Distribution
  3. In the
    Quantity
    box, type a new amount, and then click
    OK
    .
    IMPORTANT:
    If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal