Creating new states
- From theEditmenu, selectStates. TheStates Configurationdialog box opens to theLottab.TIP:You cannot edit or delete the system-definedReady To Usestate.
- If you are creating a container state, select theContainertab. If you are creating a lot state, skip this step.
- Click theNew Statebutton. TheCreate Lot (or Container) Statedialog box opens.
- In theNamebox, type a unique name for the state.
- In theDescriptionbox, type a detailed description of the state.
- TheController IDfield defaults to the next numeric value in sequence, or you can change it to a unique number. This ID is provided to allow the PLC programmer to access a sublot record from the material database.
- ClickOKto save the new state.
Provide Feedback