Removing a container

Removing a container merely unassigns the material from that container. The container definition still exists in the material database.
  1. There are three methods you can use to move containers from the
    Source Containers
    list to the
    Configured Containers
    list.
    • To remove a single container, select the container in the
      Configured Containers
      list, and then click the
      Remove
      button.
    • To remove more than one container, select the container in the
      Configured Containers
      list, hold down either the shift key or the ctrl key, select other containers to remove, and then click the
      Remove
      button.
    • To remove all the containers in the
      Configured Containers
      list, click the
      Remove All
      button.
  2. Click
    Apply
    to save the changes, or click
    OK
    to save the record and close the dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal