New server user account requirements

When creating a new user account for the
FactoryTalk Batch
or
Material Manager
Server, these requirements must be met.
  • The password must be configured never to expire--if the password ever expires, the service eventually fails to log on.
  • The user account must never be disabled or deleted--if this account is ever disabled/deleted, the service eventually fails to log on.
  • If using a domain, the domain user account must have a unique name--if the user account is a domain account, remove any local user accounts with the same name.
    TIP:
    The
    Material Manager
    Server and
    FactoryTalk Batch
    Server can use the same server user account. If they use separate accounts, the
    Material Manager
    Server account is only used on the material server computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal