Server account password change locations

If you change the password for the existing server user account, change the password in these locations:
  • Change the password for the server user account in the
    FactoryTalk Batch
    server service.
    • If you are running
      FactoryTalk Event Archiver
      in incremental mode, change the password for the server user account to the
      Batch Archiver
      service.
    • If
      e
      Procedure
      is part of your system, change the password for the server user account in the
      e
      Procedure
      Server
      service.
  • Change the password for the server user account in the
    Batch
    COM object in
    Component Services
    >
    My Computer
    >
    COM+ Applications
    .
  • If
    FactoryTalk Batch
    Material Manager
    is part of your system, change the password for the server user account in the
    MaterialTrack
    COM object in
    Component Services
    >
    My Computer
    >
    COM+ Applications
    .
    TIP:
    Make sure the server user account is a member of the MTUsers group on the Material Server computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal