Change the server user account in FactoryTalk Batch COM+ applications

To change the
FactoryTalk Batch
Server or
Material Manager
Server user account in Batch COM+ applications, complete these steps on the
FactoryTalk Batch
Server computer.
To change the server user account in FactoryTalk Batch COM+ applications
:
  1. Select
    Start >
    Windows
    Administrative Tools > Component Services
    .
  2. Expand
    Component Services
    ,
    Computers
    ,
    My Computer
    and
    COM+ Applications
    .
  3. For
    FactoryTalk Batch
    , right-click
    Batch
    , and then select
    Properties
    . The
    Batch Properties
    dialog box opens.
    • On the
      Identity
      tab, select
      This user
      and type the new
      FactoryTalk Batch
      Server user name and/or password.
    • Select
      OK
      .
  4. For
    FactoryTalk Batch
    Material Manager
    , right-click
    MaterialTrack
    , and then select
    Properties
    . The
    MaterialTrack Properties
    dialog box opens.
    • On the
      Identity
      tab, select
      This user
      and type the new
      Material Manager
      Server user name and/or password.
    • Select
      OK
      .
      TIP:
      The new permissions are applied the next time the
      FactoryTalk Batch
      Server and the
      Material Manager
      Server are started. The same server user account can be used for both servers.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal