Change the server user account for the FactoryTalk Batch Server service

To change the user account for the
FactoryTalk Batch
Server service, complete these steps on the server computer.
To change the server user account for the FactoryTalk Batch Server service
:
  1. Select
    Start >
    Windows
    Administrative Tools > Services
    . The
    Services
    dialog box opens.
  2. Right-click
    FactoryTalk Batch
    Server,
    and then click
    Properties
    . The
    FactoryTalk Batch
    Server Properties
    dialog box opens.
  3. On the
    Log On
    tab, select
    This Account
    and type the new user and/or password.
  4. Select
    OK
    .
    • If you are using
      FactoryTalk Event Archiver
      in incremental mode, change the user account name and/or password for the
      Batch Archiver
      service.
    • If
      eProcedure
      is part of your system, change the user account name and/or password for the
      eProcedure
      Server
      service.
  5. Close
    Services
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal