Static binding

If when creating a new operation or unit procedure in the Recipe Editor you select
Instance Based
in the
Unit Requirement
dialog box, you must specify a specific unit to use. During binding, the recipe must bind to that unit. Since the North_Parlor process cell has two units, you don’t want to restrict the batch to only one unit so this would not be a good type of unit binding to use.
FTBMM_GRG_equipment_requirements1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal