Material requirements: material
The unit selected to run the recipe can vary depending on the material requirement.
Example
- MBR_ADD:1 requires an addition of Material_1.
- MBR_ADD:2 requires an addition of Material_2.
- MBR_DUMP:1 has no material requirements.
Since Unit_2 does not have the ability to make an addition of Material_2, Unit_1 is selected to bind to the batch.

Provide Feedback