Material requirements: material and lot

The use of lots in the material requirement further narrows down the unit and equipment modules selected for binding.
Example
  • MBR_ADD:1 requires an addition of Material_1, Lot_5.
  • MBR_ADD:2 requires an addition of Material_3, Lot_4.
  • MBR_DUMP:1 has no material requirements.
Unit 1 is selected because it can draw from the specified lots. Unit_2 can satisfy the materials but not the specified lots.
Container_3 is a plug-flow container so the controller IDs determine which sublot is drawn from the container. Lot_4 has a smaller controller ID than Lot_8 so Lot_4 must be used first.
FTBMM_GRG_area_model_material
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal