Manual binding
Manual binding is the process of binding a unit or rebinding a previously bound unit to a step within a class-based recipe without the operator being prompted. Manual binding is done in the Procedure as SFC or Table window in the FactoryTalk Batch View while a batch is running.
With material-based recipes, the operator can direct a material-based recipe phase to:
- Bind to a material source or a material destination
- Rebind to a different material source or material destination
- Unbind from a material source or material destination
Provide Feedback