Enable Firewalls

If the InfoPlatform server is protected by a Windows firewall, the following InBound port rule needs to be configured:
New Inbound Rule
Inbound Rule Wizard
  • In the following step, provide the port that has been configured in the configuration file as described in the section. The image shows the default port setting.
  • Default port number is 12345. It is recommended to keep the default port number. To use different port for InfoPlatform Service, refer to “Change Port Number” for configuration steps.
    Inbound Rule - Protocol and Ports
    Inbound Rule - Action
  • Configure the profile according to your enterprise’s requirements.
    Inbound Rule - Profile
  • Provide the Name for the Inbound Rule and click [Finish].
    Inbound Rule - Name
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal