Post-Installation Tasks
Once the installation has been completed successfully, perform the following tasks to verify the installation to configure features of the services.
- Verify User group is created successfully.
- FTA InfoPlatform Service packages installation location.
- View the installation log.
- Disable FTASecurity.
- Additional configuration steps if the service is running with a non-administrative account.
- Enable TLS.
- Verification of running services.
- Changing the service account.
- Configuring the OPCUA Provider.
Provide Feedback