System Requirements

The hardware required for FactoryTalk Analytics InfoPlatform Service depends on the demands an application places on the system. The greater the demand, the more powerful system is required. In any application, faster processors and more memory will result in better performance. In addition, there should always be sufficient disk space to provide virtual memory that is at least twice the size of the physical memory.
Based on this, the following Server O/S requirements exist. Additional information can be found here: https://docs.microsoft.com/en-us/dotnet/framework/get-started/system-requirements
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal