Verify PI Asset Framework

  1. Log in to DataView application, under the Connection tab, click [Add Connections].
  2. Select [FactoryTalk Service] under the Rockwell Automation drop-down list.
  3. Provide the parameters and Click [Test Connection]. If all the details are valid, the “
    Test connection successful
    ” message displays.
    Test Connection
  4. Verify the list of databases, elements available under FactoryTalk Service model. DataView enables user to import and analyse EventFrames information from PIAF tags and create Storyboard.
    NOTE:
    The element tags without child items are hidden under PIAF tag hierarchy, but there is no change in the Database.
    PIAF Tags
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal