Subscription Support

InfluxDB subscriptions are local or remote endpoints to which all data written to InfluxDB are copied. InfoPlatform provides a web server endpoint as a callback endpoint to be informed by InfluxDB on all field and tag value changes. The configuration of the endpoint must be done for every InfluxDB server separately. See configurations section for more details.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal