Configure InfluxDB
This section describes the InfoPlatform InfluxDB connector. It describes configuration and user aspects of this connector.
InfoPlatform is an SDK (available as packages from NuGet) that allows for the development of applications that can include functions such as:
- Ingress data from sources on the plant floor or the enterprise.
- Model the data in hierarchical form.
- Egress the data via a RestAPI interface to web or winform based clients.
The connector described in this document is an extension of the existing solution ‘FactoryTalk Analytics InfoPlatform Service’. The connector gives the service the possibility to connect to InfluxDB. The main goal of the connector is to provide live and time-series data from InfluxDB servers.
See also: FactoryTalk Analytics InfoPlatform Service Design
Provide Feedback