Uninstallation Steps
- Open a command prompt window with administrator privileges. Change the working directory to:<DataView_HOME>\FTA Security\bin\service
- Execute the following command to uninstall the FTA Security service:service uninstall
- Delete the ES_PATH_CONF and ES_HOME in environment variable, perform the following steps:
- Execute the following command to delete the Elasticsearch Service:sc delete ElasticsearchDelete Elasticsearch Service

- Go to Start menu>Control Panel>System and Security.
- Click [System] and click [Advanced System Settings].
- Under the Advanced tab, click [Environment Variables].
- Under the System Variables section, select [ES_HOME] and click [Delete].ES_HOME - Environment Variables

- Select [ES_PATH_CONF] and click [Delete].ES_PATH_CONF - Environment Variables

- Go to theUninstallfolder in the<DataView_HOME>\Uninstalldirectory and run theUninstaller.exefile. Follow the instructions in the wizard.
- Go to Start Menu > Control Panel > Programs and Features. Uninstall the following programs:
- FactoryTalk Activation Service 4.06.13
- FactoryTalk Activation Websocket Service 2.1.1.54
- Microsoft Visual C++ 2013 Redistributable (x64)
- Microsoft Visual C++ 2013 Redistributable (x86)
- PostgreSQL 13
- FactoryTalk AnalyticsDataView
Provide Feedback