Log

The
Log
tab lists the diagnostic information of the
EtherNet/IP Address Commissioning Tool
. Use the
Log
tab to view the operation records. Only 3,000 messages can be displayed on this tab. The complete records are saved in the database. The full records can be reviewed in the exported CSV file.
Log tab actions
Button
Descriptions
Error
Used to display the error message which indicates an operation failure.
Warning
Used to display the warning message which indicates an operation is completed and it may cause a potential risk.
Information
Used to display the operation information.
Clear
Used to delete all the records in the database.
Export
Used to save the records in a CSV file.
The exported records are not limited to the 3,000 messages displayed on the
Log
tab. The CSV file contains all the records in the database.
Filter
Used to search for a specific record using key words. Case-insensitive.
Log properties
Field
Descriptions
Severity
Used to indicate the message type (
Error
,
Warning
, or
Information
) with different icons.
Time
Used to indicate when the operation happened.
Message
Used to indicate the operation record details.
TIP:
You can select any column heading to sort the list by that column.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal