Configuration
The
Configuration
tab lists the desired IP address, DHCP host name, and MAC address information for the devices being commissioned. This list is used to fulfill a BOOTP/DHCP request by matching the incoming MAC address to an item in this list. Use the Configuration
tab to add, edit, and delete the configuration list.Configuration tab actions
Button | Descriptions |
|---|---|
Add | Create a new item that includes the device Host name, IP address, MAC address, and Description. At least one MAC or IP address is required. Note :
|
Edit | Modify the selected device information. |
Delete | Remove the selected device from the configuration list. |
Commission from list | Used to guide the device startup sequence and IP address assignment process from items in the configuration list that do not have MAC addresses assigned. |
Set IP configuration mode | Used to switch the selected device IP configuration mode between Static and Dynamic. User can select one or multiples devices once. Note :
|
Import | Used to import a device list from a CSV file. |
Export | Used to save the device list in a CSV file to edit, export, and import later. |
Expand | Used to adjust the window to only view the device list. |
Filter | Used to search for a specific device using key words. Case-insensitive. |
Device properties
Field | Descriptions |
|---|---|
Host name | The DHCP device name. |
IP | The IP address for this device. |
MAC | The MAC address for this device. |
Description | The device description. |
CIP information | Indicates properties of the CIP devices, which include Vendor ID, Device Type, Product Code, Revision, Status, Serial Number, Product Name, Product Name Length, and State. It shows as Unknown if the information cannot be loaded. To get the CIP information, ensure the devices are online and then refresh the state. |
IP configuration mode | Indicates the IP configuration mode (Dynamic, Static, or Unknown) of the CIP devices. The devices need to be online The configuration modes include: Dynamic : Dynamic IP addresses are subject to change. They are assigned, as needed, by DHCP servers. If a dynamic address is not in use, it can be automatically assigned to a different device.Static : A static IP address is simply an address that does not change. Once your device is assigned a static IP address, that number typically stays the same until the device is decommissioned or your network architecture changes.To get the IP configuration mode, ensure the devices are online and then refresh the state. |
TIP:
You can select any column heading to sort the list by that column.
Provide Feedback