Blocked MAC
The
Blocked MAC
tab lists the MAC address, request count, and request time for the devices that are blocked from be assigned an IP address. Use the Blocked MAC
tab to add, edit, and delete MAC addresses.
TIP:
Go to
Settings
to enable the MAC address blocking function.Blocked MAC tab actions
Button | Descriptions |
|---|---|
Add | Used to add a MAC address to the Blocked MAC list. |
Edit | Used to modify the information of the selected device. |
Delete | Used to remove the selected devices from the Blocked MAC list. |
Import | Used to import a device list from a CSV file. |
Export | Used to save a device list in a CSV file to edit, export, and import later. |
Filter | Used to search for a specific device using keywords. It is case-insensitive. |
Expand | Used to adjust the window to view Blocked MAC Addresses only. |
TIP:
The MAC address must be unique.
Items on the
Blocked MAC
tabField | Descriptions |
|---|---|
MAC | The device's MAC address. |
Descriptions | The device description. |
Request Count | The total number of times that the device requested an IP address from the BOOTP/DHCP server. Note : The counter will reset to zero every time when the MAC address blocking function is enabled or the EtherNet/IP Address Commissioning Tool is restarted. |
Request Date | The last time that the device requested an IP address from the BOOTP/DHCP server. |
TIP:
You can select any column heading to sort the list by that column.
Provide Feedback