Change language

The default language of EtherNet/IP Address Commissioning Tool follows the operating system language. Use the language change feature to switch to the other supported language.
To change language
  1. In the title bar, click the dropdown button in the language change area, and then select a language.
  2. In the
    Language change
    dialog box, click
    OK
    .
  3. Do one of the following to make the language change take effect:
    • Restart your computer.
    • Restart EtherNet/IP Address Commissioning Tool Windows service, EtherNet/IP Address Commissioning Tool UI service, and EtherNet/IP Address Commissioning Tool.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal